May 26, 2011

TOKYO, Japan, May 26, 2011 — Renesas Electronics Corporation (TSE: 6723), a premier provider of advanced semiconductor solutions, today announced the availability of five 16-bit microcontrollers (MCUs), the RL78/I1A family, that implement in a single chip the LED control, power supply control, and communication functions required in LED lighting fixtures. The new MCUs adopt the Renesas Electronics RL78 CPU, which achieves both high computational performance and ultra low power consumption, and include from 32 to 64 kilobytes (KB) of flash memory in 20 to 38-pin package versions. These devices achieve 20 percent reduced power consumption during normal operation over the Renesas Electronics' existing 78K0/Ix2 products.

LED lighting, which features low power consumption and long lifetimes, is the focus of attention as an effort to reduce CO2 emissions on a global scale. LED illumination is becoming increasingly widely used in industrial and commercial facilities, in streetlights, and in home lighting. The global market for LED lighting equipment is expected to grow rapidly from the roughly 20 million units sold in 2009 to over 400 million units in 2014.

Given this background, Renesas Electronics has added the high-performance, ultra-low power 16-bit RL78/I1A family of MCUs to its existing 8-bit MCU lineups for use in lighting ballasts. The RL78/I1A family addresses the need of a variety of lifestyles for lower cost, high-color dimming and color temperature control. The RL78I1A supports lighting communication standards for centralized control in buildings and offices.

Key features of the RL78/I1A MCUs:

(1) Improved PWM output function for fine-grained dimming and color temperature adjustment

These new lighting MCUs provide six high-resolution PWM outputs that are capable of supporting an average resolution of 0.97 ns. This allows dimming and color temperature adjustments about 25 times more precise than RL78/Ix2 products. These new MCUs also include a new PWM output on/off control timer that allows them to support either current or PWM-based dimming adjustment.

Furthermore, these devices also include a PGA (programmable gain amplifier) that can amplify the A/D converter input level by up to a factor of 32 to support high-precision LED current measurement. Not only does this make even finer-grained brightness adjustment possible, it also allows a smaller current measurement resistor to be used, thus contributing to reduced overall system power consumption.

(2) Built-in PFC control function for reduced IC parts counts

These microcontrollers feature a newly included PFC control function that supports interleaved operation for in high-power equipment requiring improved power factors. Since the internal comparators and an interrupt pin are internally interlocked with the PWM timers, this enables efficient PFC control without CPU involvement and eliminates the need for an external PFC control IC.

(3) LED lighting safety functions

The new MCUs provide an overcurrent detection function that uses comparators (including window comparators that allow both upper and lower limits to be set) for overvoltage and overcurrent detection and stops PWM timer output automatically. This function can prevent breakdowns in lighting fixtures.

Furthermore, adopting an architecture that allows different port output states when a forcible output stop occurs to be selected from three types: high-level output, low-level output, or high impedance allows these devices to flexibly support a wide range of protection circuits.

The RL78/I1A MCUs support the IEC60730 European Home Appliance Safety Standard which is necessary for lighting fixtures by including; a FLASH memory CRC (cyclic redundancy check) calculation function, RAM parity error detection function, clock frequency detection function and illegal memory access prevention function.

(4) Lighting communication functions

In addition to CSI, these devices also support the I²C bus and UART (DMX512) standards and even the DALI (Digital Addressable Lighting Interface) open standard for lighting communication which also supports extended DALI frames. Thus they can flexibly support lighting communication needs.

Renesas Electronics positions these new products as devices that support increased functionality in LED lighting fixtures and at the same time contribute to reduced overall system costs. At the same time as promoting sales of these devices aggressively, Renesas Electronics plans to expand their lineup of MCUs that target the rapidly growing LED lighting fixtures market. The company intends to continue to release power supply and illumination solutions that make microcontroller program evaluation and design even easier.

Please refer to the separate sheet for the main specifications of the RL78/I1A MCUs.

Pricing and Availability

Samples of Renesas Electronics' new RL78/I1A MCUs are available now, priced at US$2 per unit for the 38-pin, 64 KB flash memory, 4 KB RAM version. Mass production is scheduled to begin in January 2012 and is expected to reach a combined volume of 1,000,000 units per month in 2012.

Renesas Electronics also contributes to reduced development times for lighting fixtures by releasing, starting in July 2011, the evaluation boards, automatic software generation tools (Applilet® EZ for HCD), a lighting fixture communication standard library, and other tools required for the development and evaluation of MCU software for lighting fixture applications.

(Pricing and availability are subject to change without notice.)

(Remarks) The new RL78/I1A uses SuperFlash® technology licensed from Silicon Storage Technology, Inc. SuperFlash® is a registered trademark of Silicon Storage Technology, Inc., of the U.S.A. in the United States, Japan, and other countries. Names of products or services mentioned in this release are the trademarks or registered trademarks of their respective owners. Other product and service names that appear in this press release are trademarks or registered trademarks of their respective owners

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on